This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

two 5V USB power supplies oring solution

Other Parts Discussed in Thread: LM66100, TPS2121, TPS2116

Hi team,

Do we have integrated solution for two 5V USB power supplies oring, which can be switched to the higher input voltage automatically? If not, I have to use two units of LM66100.

Thanks.

  • Hi Jerry,

    It is possible to use a PowerMUX like TPS2121 and TPS2116 in this setup. LM66100 will also work.

    Please contact the team directly for details here. We would like to understand more about the system in detail. Feel free to email me at s-dmello@ti.com