This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Unexpected waked up from sleep mode

Part Number: BQ76952

Hi team,

Our customer is facing an interesting phenomenon: The device would be waked up from sleep mode when cell voltage is less than Shutdown Cell Voltage, which I can not explain and need your help.

Attachment1 is the related log file and attachment 2 is the gg file. Thanks!

Mon Feb 08 15:28:08 CST 2021

Device Version Info = 7695_0_36
BQZ Device Name = bq76952
BQZ Firmware Version = 0_36


Sample,DateTime,ElapsedTime,ControlStatus,SafetyAlertA,SafetyStatusA,SafetyAlertB,SafetyStatusB,SafetyAlertC,SafetyStatusC,PFAlertA,PFStatusA,PFAlertB,PFStatusB,PFAlertC,PFStatusC,PFAlertD,PFStatusD,BatteryStatus,Cell1Voltage,Cell2Voltage,Cell3Voltage,Cell4Voltage,Cell5Voltage,Cell6Voltage,Cell7Voltage,Cell8Voltage,Cell9Voltage,Cell10Voltage,Cell11Voltage,Cell12Voltage,Cell13Voltage,Cell14Voltage,Cell15Voltage,Cell16Voltage,StackVoltage,PACKPinVoltage,LDPinVoltage,CC2Current,AlarmStatus,AlarmRawStatus,AlarmEnable,IntTemperature,CFETOFFTemperature,DFETOFFTemperature,ALERTTemperature,TS1Temperature,TS2Temperature,TS3Temperature,HDQTemperature,DCHGTemperature,DDSGTemperature,FETStatus,ManufacturingStatus,CellTemperature,FETTemperature,CC3Current,CC1Current,AccumCharge,AccumTime,CellBalancingActiveCells,CellBalancingPresentTime,LogRowTime(ms),LogStatus
1,2021-02-08 15:28:09,1.001,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2765,2766,2769,2771,2776,2771,2773,2778,2775,0,0,0,2792,2778,3579,9,3554,0,0x1081,0x06C2,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1622,0x0000,0,972,SUCCESS
2,2021-02-08 15:28:10,2.341,0x0000,0x04,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2711,2687,2704,2710,2717,2726,2733,2732,2739,2748,2759,0,0,0,2762,2777,3576,10,3554,0,0x1081,0x16C2,0xF881,24.8,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1624,0x0000,0,976,SUCCESS
3,2021-02-08 15:28:11,3.335,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2757,2764,2766,2769,2773,2775,2771,2773,2775,2779,0,0,0,2788,2784,3576,8,3553,-7,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1625,0x0000,0,982,SUCCESS
4,2021-02-08 15:28:12,4.369,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2764,2769,2773,2776,2771,2773,2776,2779,0,0,0,2792,2783,3576,8,3555,15,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1626,0x0000,0,978,SUCCESS
5,2021-02-08 15:28:13,5.364,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2768,2773,2776,2771,2773,2778,2775,0,0,0,2785,2784,3577,8,3553,-7,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1627,0x0000,0,984,SUCCESS
6,2021-02-08 15:28:15,6.715,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2758,2764,2766,2767,2725,2733,2732,2736,2747,2778,0,0,0,2793,2784,3577,8,3555,7,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1628,0x0000,0,962,SUCCESS
7,2021-02-08 15:28:16,7.695,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2762,2766,2768,2773,2776,2769,2774,2778,2778,0,0,0,2793,2778,3578,10,3554,7,0x1081,0x06C3,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1629,0x0000,0,981,SUCCESS
8,2021-02-08 15:28:17,8.693,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2757,2764,2766,2768,2772,2777,2771,2773,2778,2779,0,0,0,2786,2784,3577,8,3553,7,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1630,0x0000,0,968,SUCCESS
9,2021-02-08 15:28:18,9.680,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2766,2769,2774,2776,2771,2773,2776,2778,0,0,0,2791,2783,3577,8,3553,0,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1631,0x0000,0,981,SUCCESS
10,2021-02-08 15:28:19,11.030,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2763,2767,2769,2773,2773,2771,2773,2778,2777,0,0,0,2785,2783,3578,8,3553,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1632,0x0000,0,976,SUCCESS
11,2021-02-08 15:28:20,12.022,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2757,2765,2766,2769,2771,2776,2771,2773,2775,2779,0,0,0,2792,2784,3577,8,3554,7,0x1081,0x06C3,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1633,0x0000,0,982,SUCCESS
12,2021-02-08 15:28:21,13.021,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2765,2766,2767,2774,2776,2771,2773,2775,2778,0,0,0,2787,2782,3577,9,3554,0,0x1081,0x06C2,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1634,0x0000,0,968,SUCCESS
13,2021-02-08 15:28:22,14.355,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2765,2766,2767,2774,2776,2771,2773,2775,2778,0,0,0,2787,2782,3577,9,3554,0,0x1081,0x06C2,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1636,0x0000,0,1010,SUCCESS
14,2021-02-08 15:28:23,15.379,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2765,2766,2767,2774,2776,2771,2773,2775,2778,0,0,0,2787,2782,3577,9,3554,0,0x1081,0x06C2,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1637,0x0000,0,969,SUCCESS
15,2021-02-08 15:28:24,16.367,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2765,2766,2767,2774,2776,2771,2773,2775,2778,0,0,0,2787,2782,3577,9,3554,0,0x1081,0x06C2,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1638,0x0000,0,967,SUCCESS
16,2021-02-08 15:28:25,17.351,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2765,2766,2767,2774,2776,2771,2773,2775,2778,0,0,0,2787,2782,3577,9,3554,0,0x1081,0x06C2,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1639,0x0000,0,965,SUCCESS
17,2021-02-08 15:28:27,18.685,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2711,2687,2705,2766,2768,2771,2776,2771,2773,2778,2778,0,0,0,2793,2784,3576,9,3554,7,0x1081,0x06C3,0xF881,24.9,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1640,0x0000,0,977,SUCCESS
18,2021-02-08 15:28:28,19.678,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2763,2764,2766,2771,2776,2771,2772,2779,2778,0,0,0,2793,2783,3577,8,3554,-7,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1641,0x0000,0,982,SUCCESS
19,2021-02-08 15:28:29,20.676,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2762,2767,2767,2771,2774,2772,2773,2778,2778,0,0,0,2792,2783,3577,9,3553,7,0x1081,0x06C3,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1642,0x0000,0,970,SUCCESS
20,2021-02-08 15:28:30,21.664,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2766,2768,2773,2773,2771,2773,2778,2775,0,0,0,2793,2784,3577,8,3553,7,0x1081,0x06C3,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1643,0x0000,0,966,SUCCESS
21,2021-02-08 15:28:31,22.986,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2765,2766,2766,2773,2776,2771,2772,2779,2778,0,0,0,2793,2784,3577,9,3553,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1644,0x0000,0,972,SUCCESS
22,2021-02-08 15:28:32,23.979,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2763,2766,2769,2773,2775,2772,2773,2778,2778,0,0,0,2792,2778,3577,9,3553,0,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1645,0x0000,0,978,SUCCESS
23,2021-02-08 15:28:33,24.975,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2757,2764,2766,2769,2773,2777,2771,2773,2778,2775,0,0,0,2786,2784,3577,8,3553,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1646,0x0000,0,966,SUCCESS
24,2021-02-08 15:28:34,26.307,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2765,2766,2769,2773,2776,2771,2772,2778,2778,0,0,0,2792,2783,3577,8,3553,0,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1648,0x0000,0,979,SUCCESS
25,2021-02-08 15:28:35,27.302,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2764,2769,2773,2775,2771,2773,2778,2774,0,0,0,2792,2784,3576,8,3555,0,0x1081,0x06C3,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1649,0x0000,0,984,SUCCESS
26,2021-02-08 15:28:36,28.304,0x0000,0x04,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2757,2764,2766,2768,2771,2776,2771,2773,2776,2778,0,0,0,2792,2784,3576,8,3555,7,0x1081,0x16C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1650,0x0000,0,966,SUCCESS
27,2021-02-08 15:28:37,29.289,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2775,2779,0,0,0,2785,2783,3577,7,3554,-7,0x1081,0x06C2,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,-7,28,1651,0x0000,0,965,SUCCESS
28,2021-02-08 15:28:39,30.621,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2775,2779,0,0,0,2785,2783,3577,7,3554,-7,0x1081,0x06C2,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,-7,28,1652,0x0000,0,961,SUCCESS
29,2021-02-08 15:28:39,31.602,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2775,2779,0,0,0,2785,2783,3577,7,3554,-7,0x1081,0x06C2,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,-7,28,1653,0x0000,0,965,SUCCESS
30,2021-02-08 15:28:40,32.584,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2775,2779,0,0,0,2785,2783,3577,7,3554,-7,0x1081,0x06C2,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,-7,28,1654,0x0000,0,967,SUCCESS
31,2021-02-08 15:28:41,33.570,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2747,2759,0,0,0,2762,2777,3577,9,3554,-7,0x1081,0x06C2,0xF881,24.9,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1655,0x0000,0,965,SUCCESS
32,2021-02-08 15:28:43,34.903,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2763,2767,2768,2773,2774,2773,2773,2779,2778,0,0,0,2792,2783,3576,8,3553,0,0x1081,0x06C3,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1656,0x0000,0,977,SUCCESS
33,2021-02-08 15:28:44,35.900,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2757,2764,2766,2768,2771,2776,2771,2773,2778,2778,0,0,0,2792,2784,3576,9,3553,0,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1657,0x0000,0,963,SUCCESS
34,2021-02-08 15:28:45,36.883,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2766,2770,2773,2776,2771,2770,2778,2777,0,0,0,2792,2784,3577,8,3554,-15,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1658,0x0000,0,996,SUCCESS
35,2021-02-08 15:28:46,38.246,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2766,2769,2773,2776,2771,2773,2778,2775,0,0,0,2785,2784,3577,8,3554,7,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1660,0x0000,0,962,SUCCESS
36,2021-02-08 15:28:47,39.227,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2769,2773,2776,2771,2771,2778,2777,0,0,0,2791,2784,3576,8,3553,-7,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1661,0x0000,0,966,SUCCESS
37,2021-02-08 15:28:48,40.212,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2759,2765,2764,2769,2773,2775,2769,2773,2778,2778,0,0,0,2793,2778,3576,9,3554,0,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1662,0x0000,0,972,SUCCESS
38,2021-02-08 15:28:49,41.201,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2763,2767,2769,2773,2776,2771,2773,2778,2778,0,0,0,2789,2779,3576,9,3555,-7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1663,0x0000,0,990,SUCCESS
39,2021-02-08 15:28:50,42.558,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2769,2773,2776,2771,2772,2778,2778,0,0,0,2793,2784,3576,8,3554,-22,0x1081,0x06C3,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1664,0x0000,0,978,SUCCESS
40,2021-02-08 15:28:51,43.554,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2758,2765,2767,2768,2773,2776,2769,2739,2748,2759,0,0,0,2785,2783,3578,8,3553,0,0x1081,0x16C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1665,0x0000,0,982,SUCCESS
41,2021-02-08 15:28:52,44.554,0x0000,0x04,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2765,2766,2768,2773,2774,2771,2773,2778,2779,0,0,0,2792,2783,3578,9,3554,0,0x1081,0x06C2,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1666,0x0000,0,966,SUCCESS
42,2021-02-08 15:28:53,45.538,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2765,2766,2766,2773,2776,2771,2773,2778,2779,0,0,0,2792,2783,3578,9,3554,0,0x1081,0x06C2,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1667,0x0000,0,967,SUCCESS
43,2021-02-08 15:28:55,46.872,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2765,2766,2766,2773,2776,2771,2773,2778,2779,0,0,0,2792,2783,3578,9,3554,0,0x1081,0x06C2,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1668,0x0000,0,977,SUCCESS
44,2021-02-08 15:28:56,47.866,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2765,2766,2766,2773,2776,2771,2773,2778,2779,0,0,0,2792,2783,3578,9,3554,0,0x1081,0x06C2,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1669,0x0000,0,967,SUCCESS
45,2021-02-08 15:28:57,48.851,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2755,2759,2765,2766,2766,2773,2776,2771,2773,2778,2779,0,0,0,2792,2783,3578,9,3554,0,0x1081,0x06C2,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1670,0x0000,0,982,SUCCESS
46,2021-02-08 15:28:58,50.198,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2711,2687,2704,2710,2718,2726,2733,2732,2739,2748,2759,0,0,0,2762,2777,3577,9,3554,7,0x1081,0x06C2,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1672,0x0000,0,962,SUCCESS
47,2021-02-08 15:28:59,51.181,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2768,2773,2776,2771,2773,2778,2775,0,0,0,2786,2783,3577,8,3553,0,0x1081,0x06C3,0xF881,25.1,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1673,0x0000,0,965,SUCCESS
48,2021-02-08 15:29:00,52.164,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2769,2771,2776,2771,2773,2775,2779,0,0,0,2793,2783,3576,8,3555,0,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1674,0x0000,0,982,SUCCESS
49,2021-02-08 15:29:01,53.163,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2765,2766,2766,2773,2775,2769,2773,2778,2778,0,0,0,2792,2784,3576,8,3553,-7,0x1081,0x06C3,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1675,0x0000,0,967,SUCCESS
50,2021-02-08 15:29:02,54.496,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2759,2763,2767,2768,2773,2775,2773,2774,2778,2777,0,0,0,2793,2777,3576,9,3554,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1676,0x0000,0,963,SUCCESS
51,2021-02-08 15:29:03,55.479,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2766,2769,2774,2776,2772,2773,2775,2775,0,0,0,2792,2784,3576,9,3553,-7,0x1081,0x06C3,0xF881,25.4,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1677,0x0000,0,979,SUCCESS
52,2021-02-08 15:29:04,56.478,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2775,0,0,0,2793,2783,3577,8,3554,-15,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1678,0x0000,0,981,SUCCESS
53,2021-02-08 15:29:05,57.478,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2762,2766,2769,2773,2774,2772,2773,2778,2775,0,0,0,2786,2784,3576,8,3554,0,0x1081,0x06C3,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1679,0x0000,0,964,SUCCESS
54,2021-02-08 15:29:07,58.809,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2764,2766,2766,2773,2776,2771,2771,2778,2778,0,0,0,2792,2784,3577,8,3554,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1680,0x0000,0,993,SUCCESS
55,2021-02-08 15:29:08,59.818,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2763,2767,2768,2773,2773,2771,2773,2778,2778,0,0,0,2786,2784,3577,8,3553,0,0x1081,0x06C3,0xF881,25.5,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1681,0x0000,0,1014,SUCCESS
56,2021-02-08 15:29:09,60.848,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2778,0,0,0,2786,2783,3577,8,3554,7,0x1081,0x06C2,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1682,0x0000,0,968,SUCCESS
57,2021-02-08 15:29:10,62.188,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2778,0,0,0,2786,2783,3577,8,3554,7,0x1081,0x06C2,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1684,0x0000,0,973,SUCCESS
58,2021-02-08 15:29:11,63.177,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2778,0,0,0,2786,2783,3577,8,3554,7,0x1081,0x06C2,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1685,0x0000,0,968,SUCCESS
59,2021-02-08 15:29:12,64.223,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2778,0,0,0,2786,2783,3577,8,3554,7,0x1081,0x06C2,0xF881,25.2,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1686,0x0000,0,968,SUCCESS
60,2021-02-08 15:29:13,65.362,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x8184,2754,2759,2764,2766,2769,2773,2776,2771,2773,2778,2778,0,0,0,2786,2783,3577,8,3554,0,0x1081,0x16C2,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1687,0x0000,0,970,SUCCESS
61,2021-02-08 15:29:15,66.698,0x0000,0x04,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2759,2765,2766,2766,2773,2776,2771,2772,2779,2777,0,0,0,2794,2784,3578,9,3554,0,0x1081,0x06C3,0xF881,25.0,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1688,0x0000,0,978,SUCCESS
62,2021-02-08 15:29:16,67.693,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2755,2758,2764,2764,2769,2773,2776,2769,2774,2778,2778,0,0,0,2792,2784,3577,8,3554,7,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,0,28,1689,0x0000,0,983,SUCCESS
63,2021-02-08 15:29:17,68.692,0x0000,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x0184,2754,2757,2764,2766,2768,2771,2776,2771,2774,2776,2777,0,0,0,2792,2783,3577,8,3553,0,0x1081,0x06C3,0xF881,25.3,-273.2,-273.2,-273.2,22.8,-273.2,23.1,-273.2,-273.2,22.6,0x54,0x0050,22.8,-273.2,0,7,28,1690,0x0000,0,984,SUCCESS
0207-1200.gg.csv

Jayden

  • Hi Jayden,

    I'm not sure I understand the question. In the log file only Cell2 goes below the Shutdown voltage. It falls below the 2700mV 2 times for one sample each.

    In the .gg.csv file, their settings are 2700mV for Shutdown Cell Voltage, and 60 seconds for Low V Shutdown Delay. So the device should not go into Shutdown.

    Why do they have the Cell Shutdown Voltage set so high (it is higher than the under-voltage protection threshold)? If the device goes into Shutdown, it will reset all of the RAM after it wakes up again. 

    It is possible that this condition is making the device come out of Sleep. I will check with the firmware team to see if this is the case. But I recommend setting the Shutdown voltage lower than the CUV voltage.

    Best regards,

    Matt

  • Hi Jayden,

    I did notice the CUV bit is showing in the SafetyAlert register. This will cause the device to exit Sleep.

    Best regards,

    Matt