This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5569: charge pump specification

Part Number: LP5569

Hello,
I have a question about charge pump specification.

condition : cp_mode=11 ,cp_return_1x=1 ,powersave_en=1

If the VIN voltage drops once and the 1.5 x mode is turned on,

and then the VIN voltage rises due to battery charging,

is it a specification to keep the 1.5 x mode while the LED is lightening?

  • Hello,

    When setting the registers as the following:

    cp_mode=11 ,cp_return_1x=1 ,powersave_en=1

    If the VIN voltage drops once and the 1.5x mode is turned on and then the VIN voltage rises due to battery charging, charge pump will return to 1x mode while the LED is lighting.

    Best Regards 

    Monet Xu