This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2547: Difference between TPS2546 & TPS2547

Part Number: TPS2547
Other Parts Discussed in Thread: TPS2546

Hi Team,

Can someone help to double confirm that is TPS2547RTER can directly BOM 2 BOM replace TPS2546RTER ?

The only difference between them I founded was the TPS2547 has bigger continuous output current & a little bit higher IOUT short-circuit current limit, 

Are there any others I missed?

Since I found that in the following E2E thread, had been mentioned that : 

The only difference between the TPS2546 and TPS2547 is the CDP-SDP auto switch functionality. The TPS2546 enables this feature while the TPS2547 does not have this feature.

Kai Lai