Dear Sir/Madam,
Does TI have a solution similar to (TDA21472+IR35215) for 0.8V @ 200A.
The following requirements.
* Small size
* 10mVpk-pk output ripple (max)
Regards Joe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir/Madam,
Does TI have a solution similar to (TDA21472+IR35215) for 0.8V @ 200A.
The following requirements.
* Small size
* 10mVpk-pk output ripple (max)
Regards Joe
We have the CSD95490 power stage with multi-phase TPS53681 controller. More importantly, we also have an orderable evaluation board with these parts called the
TPS53681EVM-002 in stock demonstrating the capabilities you need.
Hi Josh,
Thank you for the reply.
The TPS53681 has two channels (two outputs). Is there another solution for one channel (one output)?
I could probably drop back from 200A to 160A if that opens more solutions.
Regards Joe
The simpler TPS53647 controller with one output and up to 4 phases can be used with the same CSD95490 power stages. The TPS53647 also has an orderable in stock evaluation module called TPS53647EVM-710, but its power stages are not rated for as high current as the CSD95490s.
Hi Josh,
WEBENCH limits the design to 120A. What is the maximum limit for this part?
TPS53647 data sheet, product information and support | TI.com
Regards Joe