Customer's safety team came back to me with some technical questions as shown below :
- we would like to measure/verify threshold levels for UV detection at Buck1 and buck2 output. Moreover in data sheet there’re only typical values (92% and 82%), is there a specific reason why there’s not min/max values, is it just “simulated “values ? Does it mean these thresholds are not tested in production …??? Do you still have some histograms to provide in order to have an idea what could be min/max values …?
- Can you propose a setup to measure these thresholds on the bench please ?
Thanks in advance for your support.
Best regards