Other Parts Discussed in Thread: LMR70503
Purchased a LMR70503EVM evaluation board for testing various loads with this device at -5V. The product was designed and sold by TI to produced several output voltages using a select jumper based on the LMR70503 chip. Per the documentation, no jumper should produce -5V at the output. When I tested the board without a jumper and a 3.3V input (then later at 5V) with no load on the output, the output would only reach about -3.6V and was not stable. When placing the jumper on the -2.5V that seemed to produce a stable -2.5V, as well as lower output voltages (-1.5V and -0.9V) seemed to work too.
Thinking this board was just faulty, I purchased a second unit. The second board behaved exactly as the first, and would not produce a stable output at -5V.
I created a ticket to TI Customer Support Center, asking why this product doesn't work as advertised, and here is what they said. "I just said our customer support center can't resolve your problem instead of the whole TI. Since we do not have the simulation condition we can not resolve some practical problem such yours. However on E2E Forum there are many developing engineers who can handle the difficult problems. Therefore posting on E2E forum is the best way to resolve your question." They seem to only offer help if you have a simulation of your design, but it's not my design and I couldn't seem to get that across to them.
Has anyone else seen this issue?
Shouldn't I expect TI to answer a question about their own design?