This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you said me when the reference LM61460AANRJRR will be available please ?
Regards
Hi Mickael,
I've contacted the sales engineer and have been told that it may take several months to have these parts stocked up.
Alternatively I would suggest look at the LMQ61460 which uses the same internal IC as the LM61460 but with an added benefit of having integrated high frequency bypass capacitors. The LMQ61460 is currently in stock.
Regards,
Jimmy
Thanks for your answer,
Can you confirm that the LMQ61460 is pin compatible with LMQ61440 ?
Hi Mickael,
There is no LMQ61440 available.
If you are asking if the LMQ61460 is P2P compatible with the LM61460 then yes it is.
Both devices should be VQFN-HR(14) in RJR0014A package per mechanical drawing in datasheet.
Regards,
Jimmy