Part Number: UCC28782
Other Parts Discussed in Thread: UCC24612, UCC28780
Jaden:
re: UCC28782 DITHERING FUNCTION.
Any means by which we can keep dither disabled until application/EMI tests tell us to enable it?
-r
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Robin,
The frequency-dithering function of the UCC28782 is hard-programmed into the controller and cannot be disabled by any external means.
Dithering is enabled for Ivsl currents > 646uA, which is usually at the higher input line voltages. the function "fades out" and is disabled when Ivsl < 580uA.
For the typical "universal line" input application this corresponds roughly to a 140-Vac transition boundary.
Actual input voltages depend on the transformer primary-to-auxiliary turns ratio and the upper resistor value on the VS pin.
So generally, there is no dithering during low-line operation because the bulk ripple voltage already accomplishes significant frequency deviation to spread the EMI signature. Dithering is added at higher lines where the bulk ripple is relatively low.
Regards,
Ulrich
Hello Ulrich
As usual appreciate your response: right on!
So glad to hear back from you...
Happy New Year BTW.
So we had to hop out of UCC28780/UCC24612 wagon & hitchto UCC28782/MP6908...hope we can handle the dithering events which we will have to test especially for any unforeseen events.
r
BTW: our previous pcb turned out to have 3 vias to GND plane causing all the problems! This time, we are duplicating 28782 eval kit copper plane, placement of critical parts & routing. fyi
In reply to Ulrich Goerke:
Hello Ulrich
As usual appreciate your response: right on!
So glad to hear back from you...
Happy New Year BTW.
So we had to hop out of UCC28780/UCC24612 wagon & hitchto UCC28782/MP6908...hope we can handle the dithering events which we will have to test especially for any unforeseen events.
r
BTW: our previous pcb turned out to have 3 vias to GND plane causing all the problems! This time, we are duplicating 28782 eval kit copper plane, placement of critical parts & routing. fyi
Hi Robin,
I guess this is a duplicate thread, as I have replied to the other one.
I will close this one.
Regards,
Ulrich