Other Parts Discussed in Thread: LMQ62440-Q1, LM62440-Q1, LMR36506-Q1, LM61460-Q1, LMQ61460-Q1
Hello team,
My customer has a question about overshoot that might happen while using LMR33630.
■ Product name
・ LMR33630BQRNXRQ1
・ LMR33630CQRNXRQ1
■ Usage environment
・ Vin: 14 [V], Vout: 12 [V]
* Vin varies from 4 [V] to 33 [V]. When the input is 12 [V] or less, "input voltage-(minus) voltage drop in high-side FET" will be the output.
・ The absolute maximum rating of the Vout supply destination is 16 [V]
■ Questions
They saw an article that Vout overshoots when Vin falls below the Vout set voltage at a level where UVLO (3.2 [V] on the data sheet) does not operate, and then Vin suddenly returns.
The same thing can happen with this usage assumption, so we are concerned about whether the absolute maximum rating (16 [V]) of the Vout supply destination can be met.
We would appreciate it if you could give us feedback on whether there is a problem and what to do if there is a problem.
Best Regards,
Ryotaro Fukui