Other Parts Discussed in Thread: BQ25883,
Hello,
I've finished my battery charging and gauging circuit, and I'd like to ask a few questions about it before I send the board to fabrication.
This is the circuit:
My questions are:
1) At label A: I assume that the I2C pullups should be only at the master's side, on the other side of the N1 connector. However, my concern is that if I leave the I2C pins of both chips open without pullups, noise might send unwanted data to the chips. I assume it can indeed be left open, but I'd like to make sure: Can I remove the I2C pullups (R7 and R6) from this board and leave it only at the master's side?
2) At label B: Those 2 capacitors (C12 and C13) are for ESD protection. However, note that VBAT comes directly from the BQ25883 on the same board (no connectors). I left those 2 capacitors there thinking of protection against possible ESD discharges when removing/placing batteries. But looking at it closely, it's not clear if C12 and C13 will even protect against that at all. Will C12 and C13 offer any ESD protection in this configuration? Should I just remove them?
3) What if the user plugs a cellphone charger at N2 (USB connector) with no D+/D- connection. Will the BQ25883 simply disregard D+/D- after trying communication and begin charging the battery with only the provided VBUS?
Thanks!
Eduardo