Hello Guys,
Good day.
Our customer have a list of tech inquiries for TPS1H100AQPWPRQ1 were hoping you could help us with.
1) What is the output voltage range of the current sensor? The datasheet says its 0-4V, is that correct? they are looking for a 0-5V output range for input into an ADC.
2) the chip has 3 output pins, 5,6, and 7. They are only driving a single load with this chip. Does they need to connect 5,6,7 all to the same node? Or if they connect pin 5 to the load, can they leave 6/7 floating?
3) Can the Voltage on the current sense operate in a range of 0-5V or is limited to a 0-4V range?
4) Does the PWM input need to come from a microcontroller digital output, or can they generate the PWM input using a 555 timer or some other pulse generator?
5) if the maximum current of their load can draw 3A, is this chip sufficient for an application where the load may draw 2-2.5A for sustained periods of time? If so, how can they calculate the total power dissipated by the chip?
Thanks in advance!
Art