The BQ79606 datasheet says the default UART baud rate is 250kbps (image, below). On my BQ79606 eval board, I'm seeing it default to 1 Mbps. I don't see any mention of a particular OTP programming in the eval board documentation. Also, the BQ606 documentation on the NVM is rather confusing.
Questions:
* What is the actual default baud rate of the BQ79606's UART?
* The BQ79606 documentation, in section 8.5.1.7: Non-Volatile Memory, makes mention of loading defaults from OTP from both factory and customer space. Can you explain the distinction between factory and customer space? I can't tell if this is a set of hidden/undocumented registers that get restored, or a separate page of non-volatile memory that contains factory settings, or something else entirely.
* Which registers are saved/restored by loading the OTP?
* Can the contents of the OTP memory be inspected directly, or do I have to restore it then dump all the registers?
BQ606 datasheet: