This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5390: Isolated gate driver and MOSFET circuit to control a Brushed 110V DC Series Motor

Part Number: UCC5390

Hi,

I am working on a Isolated gate driver (UCC5390SCDR) and MOSFET (STW70N60M2) based drive circuit for 110V brushed DC motor control (Split field series). In this design I would like to employ two MOSFETs where one MOSFET is for common control and other two MOSFETs are for direction control. Control has to ensured both in common and drive path. Block diagram is shown below for your reference. Does this design work for us? Please do suggest. If you share a detailed circuit with all protections, it will be appreciated.

Motor rated voltage - 110V DC, Rated current - 5A, Peak current - 8A.