This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22950: Behavior at Vin = 0V

Part Number: TPS22950


Hi Team,

Does the reverse current blocking feature of TPS22950 at 0V input conditions? More precisely, when no input voltage is present and the output sees a 5V from a micro USB port?

Thanks in advance!


Kind Regards,

Jejomar

  • Hi Jejomar,

    When there is 0V on the input, the RCB structure is powered through the output of the device. The device is able to block reverse current in the stage.

    When the input is floating, there is no internal pull down on the IN pin. In this state, RCB may or may not be triggered due to the seen voltage on the IN pin and no current path from OUT to IN.