This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: 5 LED configuration

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQSTUDIO

Hello Guys,

Good day.

Our customer just like to confirm if a 5 LED configuration works on BQ40z80? If so, should LED State of Charge status be set by "LED Support" (in bqStudio) by setting CHG and DSG Thresh 1 through 5?

Can you confirm based on sluubz5.pdf page 22 that, the sequence for the LED to go from 0% to 100% would be D8 (LED1), D7 (LED2), D12 (LED3), D11 (LED4), D9 (LED6) and D10 (LED6)?

Thanks in advance!

Art