I am planning to develop a battery balance charger which will only be connected to the cells when charging, meaning there is very limited time to achieve balance. With this in mind I would like to reduce external balance resistors to 10 ohms, to achieve 0.42A balance current. Of course I will use power resistors and rated FETs.
Would there be any issues in doing this? Would I need to change anything from the example external balance circuit? Or perhaps would a different IC be recommended for battery balance / overcharge protection?