In the Q3A Package Dimensions Drawing there are Mettalized features wich do not exist in the Q3A recommended PCB Pattern:
There is a remark 4) 'metallized features are supplier options and may not be on the package'
We have built the pad without the features and are now anxious about short circuits that could appear with the features.
Is it better to put copper keepouts in the area of the features?