Hi,
We are using TPS7B8250QDGNRQ1 in the design. Please provide response for the below queries,
1)On pg 7, the current limit is provided as 510mA. In our design, if the output is getting shorted, then we are getting the junction temperature of 173C. The thermal shutdown will happen at 175C. The junction temperature rating of LDO is 150C. Whether with 173C, it will get damaged? What will be the state of the LDO at 173C?
2)When the junction temperature reaches 175C, please provide the time taken by the LDO to enter into thermal shutdown (i.e LDO will be disabled completely)?
3)What will be the state of LDO when the junction temperature is in between 150C and 175C?
Thanks
Viswa