This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS659413EVM: Looking for 9 rails PMIC

Part Number: TPS659413EVM


Hello Team,

Our automotive customer is looking for 9-rails PMIC which sequences can be programmed freely.

They needs

Number of rails : More than 9

Voltage : 1.1V, 1.8V, 3.3V

Current : about 300mA ~ 500mA

I think TPS659413EVM can support the requirement, and the sequence can be programmable by its GUI. Is my understanding correct?

Thanks,

Yuta Kurimoto