This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3613-01: Leakage clarification

Part Number: TPS3613-01
Other Parts Discussed in Thread: TPS3619

Hello team,

The datasheet mentions that the VBAT is connected to VOUT via 15 Ohm switch.

Is this PMOS or NMOS?

If so, is the leakage lower than 100nA when VDD=3.3V and VOUT =3.0V?

I found this thread discusses about the leakage, but I'd like to make sure I_BAT specifies the leakage and it is OK for my battery.

Regards,

Itoh