Hi,
I am using a gate Driver UCC27531DBV to drive the MOSFET CSD16408Q5.The simulation results were shown below w.r.t 3.3V and 0V Input Voltages to Gate Driver.
MOSFET having Vgs = 1.4V to 2.1V.
For the MOSFET to Turn-ON, Vgs > 1.4V provided. So, Output at Load (1 Ohm) ~ 5V.
For the MOSFET to Turn-OFF Vgs < 0V provided, But still MOSFET Turned - ON and Output at Load (1 Ohm) 4.235V.
Query:
1.How to Turn-OFF the MOSFET with Gate Driver in above Circuit ?
Note: I have Downloaded the Pspice Model from TI official Website.
Thanks and Regards,
Pedaiah G.