This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM76003-Q1: Schematic review

Part Number: LM76003-Q1

Hello,

Is it possible to perform the schematic review of the attached schematic?

Thanks in advance

B.CHERDLE

2677.03.1-Power1.pdf

  • Hi

    sure, can you provide input range and output voltage?

    It looks you set at 400Khz with 5V output( the net name for TP300 is V12P0, but the FB resistor is 5V output setup), you can choose 10uH inductance with higher than 5A saturation current.  the output capacitor also need to be increased to 100uF-150uF. 

    and it is better to add some electrical capacitor too.

    Thanks

  • Hi,

    I will ask the power supply designer these datas.

    The output shall be 12V, so I think that the FB resistor couple is incorrect. I will let you know.

    Baptiste

  • Hi Baptiste:

    thanks, if 24Vin 12Vo, 15uH inductance will be recommend with 44uF-100uF output capacitance.

    Thanks

  • Hi Daniel, 

    Thanks for your reply,

    I had feedbacks from the power supply designer:

    • 12V is what we expect. R303 and R312 values have been inverted..
      • FB divider: R311 = 100K ; R312 = 9K09
      • EN divider: R302 = 100K ; R303 = 24.9K
    • all calculation have been done with a 1.5MHz frequency in the DC/DC converter. So R304 will be updated to 24.9K. In this case, the inductor value seems ok, can you confirm ?
    • Output capacitor: he calculate a 20mVpp output ripple with the 2*10uF capacitors which is enought for our design. Why more output capacitors?
    • Output current: between 0.6A and 1.8A.
    • Input voltage: arround 19V.

    schematic update extract

    Is it answering your questions ?

    Do you have additional recommandations?

    B.CHERDLE

  • Regarding input voltage, it is between 19V and 28V and can be up to  54V (in case of load dump). 

  • HI

    I will suggest using L=6.8uH or 4.7uH for 19V-28V Vin, 

    for output cap, 22uF output is fine, but cause most of ceramic capacitor will decrease by DC bias, so pls make sure the effective output capacitance under 12V is 22uF. The enough output capacitance can make the buck converter loop stable . 

    Thanks

  • Hi Daniel,

    Thanks for your reply.

    I receive feedback from our Power supply designer.

    " The DC/DC works in discontinuous current mode at 28V ; 800mA and 2.2uH. Then, we aren't in this configuration (28V) as we are connected to the battery voltage and this one decrease.

    An higher inductor value can be more confortable but the inductor size will be biggest.. 

    So we keep the 2.2uH inductor and we will see during the validation if an higher value is needed. "

    Thanks for your analysis,

    Best Regards,

    Baptiste