This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24125: If Battery charge current is at 1A, will my system load is limited to 1A

Part Number: BQ24125

Hi 

I have a question associated with BQ24125. It is based on direct connection topology, In such a system, the maximum power delivered from the external input supply to the system power bus is limited by the charger settings.

consider the example on my requirement. 

Vin: 9V

Charge current: 750mA

System load: 1.5A

From the above example my understanding as the charge current is at 750mA , it can supply only 750mA to system. 

Is it possible to achieve system load to 1.5A with charge current setting as 750mA in BQ24125.

Regards

Prabhu