Hi team,
Customer is using TPS62424 for automotive.
Their system is 5Vin, up to 300mA output and 1.8Vout at 2nd DCDC.
The datasheet specify the output voltage accuracy is -1% to 1% but they find the voltage was above than 1.8V+1% (1.818V).
-1% to 1% is rated for Vout2>2V so their output is less voltage.
- Could you share the DC output voltage accuracy for Vout=1.8V?
- Output is gradually decreased while keeping operation. Do you have temp vs Vref graph?
Best regards,
koyo