This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3898: Discharging time of CT capacitor

Part Number: TPS3898

Hi,

I need a delay time of 1 second ( -> CT = 0.25 µF) and everytime the SENSE voltage falls below VIT- I have to be sure that the capacitor is fully discharged within 10 ms. 

Will the CT capacitor be actively discharged when the SENSE voltage falls below VIT- ?

In the datasheet section 7.5  the CT pin pulldown resistance is defined with 200Ω, but i cant find any information in what context this is used? I assume this is not a constant pull down resistance, because with the 350 nA charge current the CT voltage would never get to 1.24 V.

Thanks

 

  • Hi,

    Yes, the spec of 200ohms is likely a FET pulldown resistance during normal operation.  Once the SENSE voltage falls below VIT-, the FET is turned off allowing the CT capacitor to charge up.   

    Ben