This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR62421: circuit breakdown

Part Number: LMR62421

Hi,

I have an issue with a circuit implementing LMR62421XSD/NOPB.
It is used to boost voltage from 5V to 18V. The 18V is delivered to 3 LDOs. The circuit was designed with Webench, with a small reduction of the inductance.
The circuit works fine, but breaks after some uses, currently it is tested without loads (only LDOs). With the final application the load will be <50mA, with an average of 20mA.
The supply is a bench supply of 5V, which works properly.

Have you got any suggestions or debug steps?

BR,
Nicolas