Hi,
My customer is using UCC21530-Q1 and have question on the creepage design.
They are using PCB board with CTI = 175 and want to have creepage >8mm at PCB. And I have questions below:
1. In our datasheet, it mentioned External creepage is >8mm, I assume it is for IC itself, right?
2. If customer follow our design suggestion as below, it said the creepage is 8.1mm. How could we get the number 8.1 mm stated as below.
3. How to cutout at PCB will affect the creepage numerically? Like, if the cutout is 1x10 mm. Is the creepage increased by 1 mm?
Appreciate you support in this, thank you :)
Pin