This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Is it possible to calcurate battery impedance from Ra table?

Guru 29720 points
Part Number: BQ34Z100-G1

Hi Team,

I would like to ask two questions as the following.
1)
Is it possible to calcurate battery impedance from Ra table?
Is there any calcuration formula?

2)
My customer mistaked the connection SRP and SRN in reverse.
Is there any workaround without revising their board?

Best Regards,
Yaita

  • Hello Yaita-san,

    Yes the the table is in mOhm correlating to different DOD points. You can check SLUA450 for more information.

    I'm not aware of a solution for that, the only solution would be hardware.

    Sincerely,

    Wyatt Keller

  • Hi Wyatt-san,

    Thank you for your kind support.
    I would like to ask an additional question.

    >Yes the the table is in mOhm correlating to different DOD points. You can check SLUA450 for more information.
    I believe Ra table include not only cell impedance of battery but also parasitic impedance between the device and the battery.
    Is my understanding correct?

    Best Regards,
    Yaita

  • Hello Yaita-san,

    Yes that's correct, it's the total impedance of the pack including the interconnect or other sources.

    Sincerely,

    Wyatt Keller