This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561-R2: Fuel-Gauge IC layout recommendation

Part Number: BQ27Z561-R2
Other Parts Discussed in Thread: BQ27Z561, BQ40Z50, BQ34Z100-G1

For a product I have looked for a Fuel-Gauge which can handle up to 25000mAh (1S7P) battery

I have come across BQ27Z561-xx family and they seems suitable for the product, but there is one issue on the PCB we can't have blind vias or vias in the pad and then it is impossible to rote the track to the bumps of BQ27Z561.
I there an application note available showing a recommended layout?

Or is the Fuel-Gauge available in another package?

Or can TI recommend similar fuel gauge in a package suitable for PCB's without blind vias.

The fuel gauge is for a system with embedded battery