Part Number: UCC27712
Other Parts Discussed in Thread: SN6501
Hi ,
I have selected UCC27712 for my application requirement of driving a BLDC motor.I need to apply gate pulses of format as shown in below figure to my device.
Here VT1 is my high side pulse and VT4 is my low side pulse of single half bridge.Switching frequency is 100kHz. My design stage is almost ready,but now I am encountering certain doubts.
1)For bootstrap capacitor to charge,low side device has to be turned on .Here as you can see my low side device ie. T4 gets turned on only after some duration. i.e complementary switching is not iplemented here.
So,will this circuit operate properly.Will the bootstrap capacitor hold charge for that large time and provide gate requirements to my high side device.
If I needed to apply this gate pulse pattern,is it possible for my bootstrap capacitor to provide 100% duty or do I need some additional charge pump circuitry.
Regards,
Reshma