Other Parts Discussed in Thread: SN6501, UCC27201, UCC27282
Hi all,
I'm thinking to use two of your UCC27282-Q1 to drive a Full H-Bridge like showed in the following image ( the inductor represents a brushed motor ):
Is it possible to use a PWM with 100% duty cycle in this configuration?
Can I keep the High mosfet at level high indefintely, or after some time the boot capacitor discharges and the high mosfet turns off?
In this example I use the low mosfets for choppering, is it better to use the high mosfets?
Regards,
Lorenzo