This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM846C23: PMBus configuration with external resistor

Part Number: TPSM846C23


Not clear to me how the PMBus control and the Ext resistor work together.

I assume we have to use an external R to set the nominal, otherwise will start up the first time at 0.5v and it won't be able to turn on the downstream component.

  • We want a 0.9v default and expect to adjust down to 0.85 via PMBus.

I can put a 12.1K res on the RSet to get 0.9 nominal. But not clear if that changes the mapping from code to voltage on the VOUT register.

  • Will it still be Vout = code * 512?
  • Will the PMBUS host do the right thing to adjust the output voltage even with the RSet in place (does PMBus override the Rset value)?

Thanks,
Nick