This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122ZA: Reference design for negative input to high positive output

Guru 19645 points
Part Number: LM5122ZA
Other Parts Discussed in Thread: LM5122,

One customer is considering below 2-phase interleaved power supply.

Is there any reference design for two pattern below?

①Vin: DC -48V (-36~-60V) ⇒ Vout: DC 32V, Iout: 31.25A (1kW)

②Vin: DC -36~-46V ⇒ Vout: DC 54V, Iout: 18.52A (1kW)

 

I think that DC/DC controller is mainly LM5122 or LM5122ZA.

If there more recommend controller, please let me know.

Best regards,

Satoshi