This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25221: Is ESD Protection Necessary?

Part Number: TPS25221

Hello,

Typically if I had a buck converter IC passing +5V to an outward facing port, I would not include an ESD diode on the +5V line. (I'm thinking the LC filter sufficiently protects the IC from any ESD strikes that happen on the port?)

However, if I put an IC like the TPS25221 between the buck IC and the port, it seems like the TPS25221 is now vulnerable. All the EVMs I checked don't have an ESD device on the output of the USB switch IC, but there is the 150uF capacitor for USB compliance.

  1. Is the 150uF enough to absorb ESD strikes and protect the IC?
  2. We don't need USB compliance for our application. If we remove the 150uF capacitor, is it necessary to now add discrete ESD protection?
  3. Is the native ESD protection built into the IC enough to protect it under normal circumstances?

Thank you!

  • Hi Sir/Madam,

    It can pass the IEC ESD +-8kV contact and +-15kV air discharge.

    It's suggested to add at least 10uF+0.1uF at output.

    For TI's policy, I will first click resolved button.

    If you have any other concern, contact me any time.

    If you think resolved, please help click 'Issue is solved button'.

    Thanks.