Part Number: BQ25505
Hi Team,
Customer now use BQ25505 in watch display. The BQ25505 is used as a relay boost for the solar panel to charge the watch battery.
The maximum voltage of solar energy is around 0.7V, and solar energy charges the battery through ICBQ25505;
The rated voltage of the battery is 4.35V. On the schematic, BAT_4V2 is directly connected to the battery. The power supply for the entire board is output from pin 19 of BQ25505, and the signal is VBAT. The overvoltage alarm is set to 4.50V.
Could you kindly help to check whether the SCH is ok?