Other Parts Discussed in Thread: BQ79616,
Hey team,
I had a customer who was originally looking at the BQ79616, but due to lead time is looking to some other options to begin prototyping with. This resulted in some questions related to the BQ76PL455A and BQ89606. The questions are as follows:
- If I used the BQ79606 as a bridge IC, would it be able to communicate with the 76PL455A using the capacitive communication architecture? They appear to be the same interface (almost the same protocol format). I'm not sure if there's been hardware improvements between the families that would prohibit this kind of operation.
- I recall the BQ76PL455a having distancing limitations with the capacitive communication interface (based on wiring, filters, etc). What are the limits of the BQ79606 and BQ79616? As I understand it, the interface should implement at a minimum capacitive isolation and dual chokes or isolation transformers to get the best performance at cable distances greater than 2m. How far beyond 2m is possible? 10m, 25m more? For instance, in the BQ79606 datasheet, it specifies how to calculate the daisy chain cable capacitance. Maybe I'm missing something, but I didn't find a call out for the capacitance limit. The Bq79616 datasheet doesn't mention anything about cable capacitance as well.
- For the BQ79606, 79616, and 76PL455A, as messages travel up and down the capacitive communication bus, if devices are connected to the UART (ie MCU), would those devices also see the message? If so, could they theoretically respond as well by responding back over the UART
I appreciate your feedback!
Cameron