Other Parts Discussed in Thread: TPS543C20, TPS543C20EVM-869
Hello,
We are considering using the TPS543B20 in stackable mode in one of our designs in order to make use of the phase shift functionality of the part. The synchronization frequency we would like to provide as the clock is nominally 1 MHz, but with tolerances, could be slightly in excess of 1 MHz. Do you know if there is an upper limit on the input clock frequency of the TPS543B20 when operating in stackable mode? It would appear that the 1 MHz value listed in the datasheet is the maximum allowable value, but I would like to confirm this if possible.
Thanks,
Adam