Hi Team,
When scaling the BQ78350-R1 via the current calibration method, does the scale factor also need to be applied to the Electronics Load parameter? I.e. if a 10A load is used for calibration but is input as 250mA for 40x scaling, should Electronics Load be set to 33 (~100uA) for a 4mA target? I believe this is how it is done when using IPScaling on -R2, but want to confirm that it applies when scaling this way as well.
Thanks,
Antonio