This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV841: TI solution suggestion

Part Number: TLV841


Dear Team,

Could you/ give me some suggestion for Reset IC? We appreciated your great support.

Reset IC with 2.6v threshold ,open-drain output, >=100ms fix delay, and sot23-3 package.

Many Thanks

Jimmy

  • Hello Jimmy,

    Thank you for checking on latest offering TLV841.

    TLV841 is a WCSP package supervisor. Based on your query, can I assume you are not looking for WCSP package solution?

    For your requirement of 2.6V threshold, Open Drain output, >=100ms fix delay, SOT23-3 package, I can recommend following options

    TLV803EA26DBZR - 2.64V threshold, 200msec fixed delay

    TLV803EA26RDBZR - Same as above but with different pinout

    TLV803EF2DBZR - 2.64V threshold, 400msec fixed delay

    Let us know if these options are acceptable.

    Thanks & Regards,

    Shridhar