Hello All,
I am using UCC28634 for 150V-265VAC to 5.00VDC @ 6A
The circuit and transformer specs are as per TI webench reports
The circuit output is 5V at no load Connected
as soon as I connect a resistive load for example a 10-ohm resistor ()
the output voltage drops to zero
and I can hear an audible noise in form of ticking across the transformer
attaching images of output voltage in both the conditions
I think the controller does not change the PWM frequency for MOSFET even if there are changes in output current
I am also attaching the circuit Diagram and transformer reportCoreCoilformer23.pdf