Part Number: LM2759
Hi,team
My customer has a question.
The LED current sink accuracy is only specified at 220mA flash mode in the datasheet.
Could you please tell the accuracy for torch mode 15mA?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2759
Hi,team
My customer has a question.
The LED current sink accuracy is only specified at 220mA flash mode in the datasheet.
Could you please tell the accuracy for torch mode 15mA?
Thank you.
Hi Sean
Thank you for your reply.
My customer made about 100 devices incorporating the LM2759SD.
The device operates in torch mode 15mA, Flash mode 150mA and 280mA.
In Flash mode 150mA and 280mA, the current error is within ± 10%.
But with the two devices, the current in torch mode 15mA was 6.7mA and 8.3mA.
Do you think these two LM2759s are normal or damaged?
Condition: One LED is connected to the LM2759DS. Vin of LM2759 is about 3.8V. Vf of LED is about 2.6V at If 15mA .
Regards,
Jenny
Hi Jenny,
Thanks for the detail explaination, as you know for such device, we can only guarantee the current accuracy under full scale current and we cant' guarantee the current accuracy for the whole current range.
BR
Sean