This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: ILIMT/ICHG setup

Part Number: BQ25606

Hi TI Team,

I have a question about BQ25606 as below. The D+ and D-  of BQ25606 is floating. We use MCU to communicate with USB 3.0. 

Input = USB 3.0 (5V/0.9A)

ILIM setup = 900mA 

ICHG setup = 800mA

System output load = 150 mA

Is it possible to trigger OCP of USB 3.0 ? 

Shawn