This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A11: Output capacitance when driving an FPGA

Part Number: TPS7A11


All,

One of my customers is using the TPS7A11 to power an FPGA rail. Maximum output capacitance for the TPS7A11 is 22 uF; minimum capacitance at the input of the FPGA is 47uF + 4 100 nF, trace is about 1 cm. What is recommended here.

 

Thanks,

Regards,

Joe