I am using LM3481 controller IC for SEPIC converter design. The sepic parameters are: Vin: 6.5 -40V, Vout: 18V, Iout: 1A. Currently we have supply at input of LM3481 same as Vin of SEPIC. I want to check the maximum values of junction temperature and IC supply current at high operating temperature (105 deg C) to see if there are any issues at 40V supply input voltage to the IC. The maximum supply current, junction temperature etc.. values given in the datasheet are at Vin=12V and temp 25 deg C. What values do we use at 105 deg C and 40V supply input to the IC?