This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCSEL DRIVER IC

I'm going to use two VCSELs in series.

I'm trying to control PWM.

Please recommend a DRIVER IC that can be used.

VCSEL information is as follows

VCSEL : V107C051A-940 A01

               IF : 5.8A

               VF : 2.1V

               Quantity : 2 EA (Serial Configuration)

Input Power : 7V

We would appreciate it if you could provide us with an applicable driver ic and configuration circuit.