This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: Efficiency of TPS63070

Part Number: TPS63070


Hello Team,

My customer would like to know more information about the Efficiency of TPS63070. Using this device and with the same circuit as given in the schematic on page 1 of the datasheet and using the recommended components. The input voltage is 3.6V and the output is 3.3V. At low currents (about 4 mA). They are seeing an efficiency of around 50%. Is this correct?

When PS/SYNC is tied high. In Table 7 and Figure 12 it seems to indicate that when PS/SYNC is high the device is in PWM mode and efficiency is very low at low current levels - sub 1mA. While in Figure 13 the efficiency is much higher.

Regards,

Renan