Other Parts Discussed in Thread: TIDA-050047
Hi,
We are planning to use BQ25792 in our new design.
I would like to know that whether we can use this module with an DC supply of 12V-24V instead of VBUS option from USB connector?
So there will be no D+/D- signals as there is no USB option.
As per the datasheet section 8.3.4 Device Power Up from Input Source, the charger performs D+/D- detection and after that only will start charging or switch power to SYS.
But as per the reference design TIDA-050047, the D+ and D- pins are NC.
- Can I keep the D+ and D- as NC and use the charger without D+/D- detection?
But as per the datasheet if the BQ25792, the recommended maximum IVBUS is 3.3A.
As per the Type-C power Delivery, 100W is achieved by 5A @20V.
- I want to know whether BQ25792 can support input current (IVBUS) more than 3.3A.
- Also please suggest what is the maximum output current that charger can provides through Pin SYS either from battery or VBUS
Shafeeq