Hi expert,
My customer try to use a external DC source as a charging input( not a adapter) 5V3A, they want to know how to limite the charging current to 1A. according to datasheet , I think the first step is limiting input current to 2A or 1A by setting D+ D- to below threshold. then use I2C to set the Charge Current Limit register(REG02) . is this a right approach? I don't have a EVM board on hand yet. BTW, What's the sugguestion how to set D+ D- Threshold? is there a recommended circuit? thanks.