This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25302: BQ25302 Standalone Battery Charger PMID

Part Number: BQ25302


Hi

If VBUS do not have power supply, does the discharge path correct?  Battery --> buck inductor --> Q2 -->PMID ---> System

Does Q2 fully turn on or use the diode? If take this path, is there a current limit?

Thanks

Star

  • Hi Star,

       Yes there is a path through the diode of the HSFET. On battery only the converter will not be on due to SLEEP mode so Q2 would not be on. There is no discharge current limit as the body diode orientation means even if you turn the FET off, it won't block the discharge current limit. There is also the ability shown in the datasheet to use an external FET to connect BAT and SYS.